Αναζήτηση

Έναρξη κύριων περιεχομένων

  • Καταχώρηση
  • Είσοδος

Υπηρεσίες

Print page

Υπηρεσίες

Ans/QNAS > iQ Platform

A/QnA and AnS/QnAS platforms have been Mitsubishi Electric's main control technology for many years. However, these technologies are now obsolete as many electrical components have reached their end of life.

For that reason, already some years ago Mitsubishi Electric with its iQ Platform offered a successor technology, now being a leading control solution providing faster and more reliable controllers than before. On top of that iQ Platform provides many modern features that allow our customers to meet the requirements of the digitalization era.

Mitsubishi Electric provides a set of software and hardware tools to support the process of transition to the new technology, including special adapters to keep the existing wiring as well as PLC program converters.

Transition process

  • Identify the install base of obsolete technology
  • Identify the communication network used. It might be possible to make the transition in stages where new controllers communicate with old ones.
  • Identify system requirements and available budget
  • Contact Mitsubishi Electric’s technical support if needed

Catalogs

AAnS iQ-R Upgrade Tool (pdf)

Programmable Controller Upgrade Tool General Catalog (pdf)

MELSEC iQ-R Series Upgrade Tool (pdf)

MELSEC A to Q Series Upgrade tool (pdf)

Guidebooks

Transition MELSEC A to Q series (ZIP)

MELSEC-AQnA Small type to iQ-R Series Handbook (PDF)

MELSEC-AQnA Large type to iQ-R Series Handbook (PDF)

MELSEC A/QnA to MELSEC iQ-R Conversion Support Tool

MELSEC A/QnA to MELSEC iQ-R Conversion Support Tool converts a GX Developer format project into a GX Works3 format project. This tool can also output support information which is necessary to correct the converted project. Please refer to the corresponding operating manual for more information.

MELSEC A/QnA to MELSEC iQ-R Conversion Support Tool (ZIP)

MELSEC A/QnA to MELSEC iQ-R Conversion Support Tool Operating Manual (PDF)

MELSEC A/QnA to MELSEC Q Conversion support tool

The conversion support tool minimizes the efforts when migrating to Q technology. Simply change the PLC type in your project and the tool will highlight differences between two programs. It also provides guidance on how to complete the conversion.

MELSEC A/QnA to MELSEC Q Conversion support tool (ZIP)

Other supporting data

Videos

How to replace a MELSEC A-series PLC with MELSEC Q series using a base adapter (MP4)

How to replace a MELSEC A-series PLC with MELSEC Q series using a Q type base unit (MP4)

Manuals

For more technical details about the AnS and QnAS Platforms, please find the respective manuals in our Download Centre

Manuals

Αρχή